This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61027: TPS61027DRCR - This boost converter not working for 200mA load.

Part Number: TPS61027
Other Parts Discussed in Thread: TPS61033, TPS61022

Tool/software:

Hi Team,

In my design, the input voltage (Vin) is fixed at 3.3V, and the output voltage (Vout) is set to 5V using the TPS61027DRCR boost converter. The load current is 200mA. When the device is powered on with the load connected (drawing 200mA), the output voltage remains at 0V and does not reach 5V. However, if the load is disconnected during power-up and then connected after startup, the output reaches 5V as expected.

I also tested this behavior on the EVM and observed the same issue.

Let me know if you want help diagnosing the root cause or fixing the circuit or is it normal behavior? If it is normal behavior, why you haven't mentioned anything detailed? and mentioned for 1500mA?

Looking forward your quick response!

Thanks 

Murali