Other Parts Discussed in Thread: LMG2100R044
Tool/software:
Hi,
According to LMG2100R044 datasheet, AGND and PGND pins are internally connected. I could also confirm it by desoldering the external jumper in the EVM (R10) that connects those grounds.
My questions are:
1. If the pins are internally connected, then what is the need to connect them externally? I read somewhere in the forum that it is for debugging purposes when the device is not installed on the board. Is this the only reason?
2. Why the R10 resistor in the EVM is laid out far away from the device? isn't it a possible cause for ground loops?
Thank you in advance for your help,
Erfan