Other Parts Discussed in Thread: AM4378
Tool/software:
Hello experts
Hope this finds you well.
We want to confirm the max output current
BQ24072T will be used in the boards equipped with TI AM4378.
What is the upper limit of the current that can be output when the system is operating during charging?
The data sheet of this charging IC states that the input current @in pin is 1.5A (max) and the output current @out pin is 4.5A (max).
If the system is operated while charging, is it correct to think that the input current of the charging IC + the battery output current <= 4.5A
Also, is the output current limited to 1.5A when the battery is empty
Thank you
Regards,
Zhou