This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92201: LED glows slightly when EN is High and PWM is Low (0% Duty)

Part Number: TPS92201


Tool/software:

Hello,

In my TPS92201 circuit, I have the EN pin pulled High and the PWM pin held Low (0% duty cycle, tied to GND). Based on the datasheet, I expect the device to be enabled but the LEDs to remain completely off due to 0% PWM input.

However, I observe that the LEDs are slightly glowing even when the PWM is Low.
Is this expected behavior? Could this be due to noise or leakage current on the PWM or SW pin?
Any recommendations on how to ensure the LEDs remain fully off in this state?

Thank you!