Tool/software:
Dear team,
may LM74502-Q1 be used for surge protection and regulation?
İf a diode connected to input for reverse polarity, Q2 is unneccessary, is that right?
if input voltage is 48 volt and R2 and R3 is arranged to clamp voltage around 30V, Or Dz clamp voltage is choosen 30V, LM74502-Q1 acts like a regulator, is there any unsufficent situation?
which one is sufficient, Arranging R2 and R3 to clamp voltage around 30V or Choosing Dz clamp voltage 30V?
Of course Q1 will be choosed to dissepate enough power.
the circuit which is on figure 10-11 on datasheet, is not needed tvs for load dump, Because VS pin is protected with DZ and R1, is that right?
Best Regards.