Tool/software:
Hi team,
My customer has been considering BQ79616-Q1 for functional safety application. Could you please kindly answer the questions below?
The cells have the function which automatically stops the charging and the discharging when overcharging condition is detected. My customer assumes BQ79616-Q1 gets broken due to this function. If there is an abnormal mode in which the BQ79616-Q1 continues to produce voltage data with a normal value that is different from the actual cell voltage, the system cannot stop charging and discharging.
1. Is there an abnormal mode of BQ79616-Q1 that continues generating data that is different from the actual cell voltage?
2. Is it possible for BQ79616-Q1 to detect the operation of 1 by self-diagnosis, etc. and notify it to MCU by communication?
Best regards,
Shunsuke Yamamoto
Figure found at the