This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS6507x datasheet: circuit example error

Anonymous
Anonymous

Other Parts Discussed in Thread: TPS65070, TPS3805H33

Hi,

I would like to ask a question on TPS65070.

  1. In its datasheet slvs950d, page 71, Fig. 49, [Sense] pin of TPS3805H33 is directly connected to DVDD3318 pins of OMAP L138.
  2. In its application report slva371b, page 4, Fig.1, [Sense] pin of TPS3805H33 is connected to DVDD3318 pins of OMAP L138 via resistor divider.

In think (1) is wrong because according to SLVS392A, TPS380x datasheet, [Sense] pin of TPS3805H33 has threshold voltage of 1.226V, therefore a resistor divider must be required from either 3.3V or 1.8V voltage supply out of TPS65070's DCDC2. This is however missing in (1).

Could anyone confirm this?

 

Zheng