This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61096A: I am struggling to design 30V to 150V boost converter with 1A current output

Part Number: TPS61096A
Other Parts Discussed in Thread: LM5155

Tool/software:

I'm working on a project that requires designing a boost converter to step up from 30V to 150V DC with an output current of 1A. Considering efficiency losses, I'm planning for an input current of around 1.2A.

I came across a reference circuit in an application note using the TPS61096A IC, but it seems like this IC may not support the required output current of up to 1A at 150V.

Can anyone recommend a suitable DC-DC boost converter IC for this application? Ideally, I'd love to see a reference design or evaluation module to help speed up the development process.

Thanks in advance for your suggestions!