Other Parts Discussed in Thread: MSP430FR2355
Tool/software:
Good afternoon, currently I have been having issues with my IC and MCU communicating with I2C which I am not sure where it is stemming from. I am using an MSP430FR2355 as used in the example code for the IC and am not seeing anything happen. Initially I was running the code using pins 4.6 and 4.7 for SDA and SCL however for some reason I had to abandon it as the SDA pin does not pull high and instead pulls up to 2.38V rather than 3.3V like the SCL pin. I have a 10K pull up resistor and the 3.3V source coming from the REG1 pin as I am using the bq7695202 where REG1 is 3.3V by default. What perplexes me is that I was initially seeing SCL come on and be a bit off on the KHz time however now I am not seeing anything. I switched to the 1.2 and 1.3 UCB0 side for I2C and think I changed the code right but am not seeing anything happen. I do however see the pins pull low after the GPIO and I2C pins are initialized but after the line " P1SEL1 &= ~(BIT2 | BIT3);" where the pins are initialized the pins are pulled back high to 3.3V which is normal. When it hits the I2C ISR on the 4.6 and 4.7 side it would go to vector 24 and stop at bis in the I2C write function, yet now it does not go to vector 24 and instead hits the switch in the ISR and skips the case statement and go directly to the last line in the ISR. I have tried to see it in a logic analyzer and have not seen anything. Could you help me? I will attach my current code initialized for 1.2 and 1.3 below. THanks!
// Includes #include <msp430.h> #include <stdio.h> #include <stdint.h> #include <stdbool.h> #include <HAL.h> #include <QmathLib.h> //#include <Include/callbacks_mpack.h> #include "BQ769x2Header.h" // Defines #define DEV_ADDR 0x08 // BQ769x2 address is 0x10 including R/W bit or 0x8 as 7-bit address #define CRC_Mode 0 // 0 for disabled, 1 for enabled #define MAX_BUFFER_SIZE 10 #define R 0 //Read #define W 1 //Write #define W2 2 //write data with two bytes // Arrays uint8_t RX_data [2] = {0x00, 0x00};// used for DirectCommand func, uint8_t RX_32Byte [32] = {0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00}; //****************************************************************************** // I2C State Machine *********************************************************** //****************************************************************************** typedef enum I2C_ModeEnum{ IDLE_MODE, NACK_MODE, TX_REG_ADDRESS_MODE, RX_REG_ADDRESS_MODE, TX_DATA_MODE, RX_DATA_MODE, SWITCH_TO_RX_MODE, SWITHC_TO_TX_MODE, TIMEOUT_MODE } I2C_Mode; /* Used to track the state of the software state machine*/ I2C_Mode MasterMode = IDLE_MODE; /* Register address/command to use*/ uint8_t TransmitRegAddr = 0; /* ReceiveBuffer: Buffer used to receive data in the ISR * RXByteCtr: Number of bytes left to receive * ReceiveIndex: The index of the next byte to be received in ReceiveBuffer * TransmitBuffer: Buffer used to transmit data in the ISR * TXByteCtr: Number of bytes left to transfer * TransmitIndex: The index of the next byte to be transmitted in TransmitBuffer */ uint8_t ReceiveBuffer[MAX_BUFFER_SIZE] = {0}; uint8_t RXByteCtr = 0; uint8_t ReceiveIndex = 0; uint8_t TransmitBuffer[MAX_BUFFER_SIZE] = {0}; uint8_t TXByteCtr = 0; uint8_t TransmitIndex = 0; //****************************************************************************** // BQ Parameters *************************************************************** //****************************************************************************** // Global Variables for cell voltages, temperatures, Stack voltage, PACK Pin voltage, LD Pin voltage, CC2 current uint16_t CellVoltage [16] = {0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00}; float Temperature [3] = {0,0,0}; uint16_t Stack_Voltage = 0x00; uint16_t Pack_Voltage = 0x00; uint16_t LD_Voltage = 0x00; uint16_t Pack_Current = 0x00; uint16_t AlarmBits = 0x00; uint8_t value_SafetyStatusA; // Safety Status Register A uint8_t value_SafetyStatusB; // Safety Status Register B uint8_t value_SafetyStatusC; // Safety Status Register C uint8_t value_PFStatusA; // Permanent Fail Status Register A uint8_t value_PFStatusB; // Permanent Fail Status Register B uint8_t value_PFStatusC; // Permanent Fail Status Register C uint8_t FET_Status; // FET Status register contents - Shows states of FETs uint16_t CB_ActiveCells; // Cell Balancing Active Cells uint8_t UV_Fault = 0; // under-voltage fault state uint8_t OV_Fault = 0; // over-voltage fault state uint8_t SCD_Fault = 0; // short-circuit fault state uint8_t OCD_Fault = 0; // over-current fault state uint8_t ProtectionsTriggered = 0; // Set to 1 if any protection triggers uint8_t LD_ON = 0; // Load Detect status bit uint8_t DSG = 0; // discharge FET state uint8_t CHG = 0; // charge FET state uint8_t PCHG = 0; // pre-charge FET state uint8_t PDSG = 0; // pre-discharge FET state uint32_t AccumulatedCharge_Int; // in AFE_READPASSQ func uint32_t AccumulatedCharge_Frac;// in AFE_READPASSQ func uint32_t AccumulatedCharge_Time;// in AFE_READPASSQ func //****************************************************************************** // Function prototypes ********************************************************* //****************************************************************************** void GPIO_initPins(void); void GPIO_configPins(void); void UCS_initModule(void); void I2C_initModule(void); void UART_initPins(void); void Software_Trim(void); void delayUS(uint16_t us) { // Sets the delay in microseconds. uint16_t ms; char i; ms = us / 1000; for(i=0; i< ms; i++) __delay_cycles(16000); } void CopyArray(uint8_t *source, uint8_t *dest, uint8_t count) { uint8_t copyIndex = 0; for (copyIndex = 0; copyIndex < count; copyIndex++) { dest[copyIndex] = source[copyIndex]; } } unsigned char Checksum(unsigned char *ptr, unsigned char len) // Calculates the checksum when writing to a RAM register. The checksum is the inverse of the sum of the bytes. { unsigned char i; unsigned char checksum = 0; for(i=0; i<len; i++) checksum += ptr[i]; checksum = 0xff & ~checksum; return(checksum); } unsigned char CRC8(unsigned char *ptr, unsigned char len) //Calculates CRC8 for passed bytes. Used in i2c read and write functions { unsigned char i; unsigned char crc=0; while(len--!=0) { for(i=0x80; i!=0; i/=2) { if((crc & 0x80) != 0) { crc *= 2; crc ^= 0x107; } else crc *= 2; if((*ptr & i)!=0) crc ^= 0x107; } ptr++; } return(crc); } I2C_Mode I2C_ReadReg(uint8_t reg_addr, uint8_t *reg_data, uint8_t count) { /* Initialize state machine */ MasterMode = TX_REG_ADDRESS_MODE; TransmitRegAddr = reg_addr; RXByteCtr = count; TXByteCtr = 0; ReceiveIndex = 0; TransmitIndex = 0; /* Initialize device address and interrupts */ UCB0I2CSA = DEV_ADDR; UCB0IFG &= ~(UCTXIFG + UCRXIFG); // Clear any pending interrupts UCB0IE &= ~UCRXIE; // Disable RX interrupt UCB0IE |= UCTXIE; // Enable TX interrupt UCB0CTLW0 |= UCTR + UCTXSTT; // I2C TX, start condition __bis_SR_register(LPM0_bits + GIE); // Enter LPM0 w/ interrupts //For debugger __no_operation(); /* Copy over received data */ CopyArray(ReceiveBuffer, reg_data, count); return MasterMode; } I2C_Mode I2C_WriteReg(uint8_t reg_addr, uint8_t *reg_data, uint8_t count) { /* Initialize state machine */ MasterMode = TX_REG_ADDRESS_MODE; TransmitRegAddr = reg_addr; /* Copy register data to TransmitBuffer */ CopyArray(reg_data, TransmitBuffer, count); TXByteCtr = count; RXByteCtr = 0; ReceiveIndex = 0; TransmitIndex = 0; /* Initialize device address and interrupts */ UCB0I2CSA = DEV_ADDR; UCB0IFG &= ~(UCTXIFG + UCRXIFG); // Clear any pending interrupts UCB0IE &= ~UCRXIE; // Disable RX interrupt UCB0IE |= UCTXIE; // Enable TX interrupt __no_operation(); UCB0CTLW0 |= UCTR + UCTXSTT; // I2C TX, start condition __bis_SR_register(LPM0_bits + GIE); // Enter LPM0 w/ interrupts //For debugger __no_operation(); return MasterMode; } void BQ769x2_SetRegister(uint16_t reg_addr, uint32_t reg_data, uint8_t datalen) { uint8_t TX_Buffer[2] = {0x00, 0x00}; uint8_t TX_RegData[6] = {0x00, 0x00, 0x00, 0x00, 0x00, 0x00}; //TX_RegData in little endian format TX_RegData[0] = reg_addr & 0xff; TX_RegData[1] = (reg_addr >> 8) & 0xff; TX_RegData[2] = reg_data & 0xff; //1st byte of data switch(datalen) { case 1: //1 byte datalength I2C_WriteReg(0x3E, TX_RegData, 3); delayUS(2000); TX_Buffer[0] = Checksum(TX_RegData, 3); TX_Buffer[1] = 0x05; //combined length of register address and data I2C_WriteReg(0x60, TX_Buffer, 2); // Write the checksum and length delayUS(2000); break; case 2: //2 byte datalength TX_RegData[3] = (reg_data >> 8) & 0xff; I2C_WriteReg(0x3E, TX_RegData, 4); delayUS(2000); TX_Buffer[0] = Checksum(TX_RegData, 4); TX_Buffer[1] = 0x06; //combined length of register address and data I2C_WriteReg(0x60, TX_Buffer, 2); // Write the checksum and length delayUS(2000); break; case 4: //4 byte datalength, Only used for CCGain and Capacity Gain TX_RegData[3] = (reg_data >> 8) & 0xff; TX_RegData[4] = (reg_data >> 16) & 0xff; TX_RegData[5] = (reg_data >> 24) & 0xff; I2C_WriteReg(0x3E, TX_RegData, 6); delayUS(2000); TX_Buffer[0] = Checksum(TX_RegData, 6); TX_Buffer[1] = 0x08; //combined length of register address and data I2C_WriteReg(0x60, TX_Buffer, 2); // Write the checksum and length delayUS(2000); break; } } void CommandSubcommands(uint16_t command) //For Command only Subcommands // See the TRM or the BQ76952 header file for a full list of Command-only subcommands { //For DEEPSLEEP/SHUTDOWN subcommand you will need to call this function twice consecutively uint8_t TX_Reg[2] = {0x00, 0x00}; //TX_Reg in little endian format TX_Reg[0] = command & 0xff; TX_Reg[1] = (command >> 8) & 0xff; I2C_WriteReg(0x3E,TX_Reg,2); delayUS(2000); } void Subcommands(uint16_t command, uint16_t data, uint8_t type) // See the TRM or the BQ76952 header file for a full list of Subcommands { //security keys and Manu_data writes dont work with this function (reading these commands works) //max readback size is 32 bytes i.e. DASTATUS, CUV/COV snapshot uint8_t TX_Reg[4] = {0x00, 0x00, 0x00, 0x00}; uint8_t TX_Buffer[2] = {0x00, 0x00}; //TX_Reg in little endian format TX_Reg[0] = command & 0xff; TX_Reg[1] = (command >> 8) & 0xff; if (type == R) {//read I2C_WriteReg(0x3E,TX_Reg,2); delayUS(2000); I2C_ReadReg(0x40, RX_32Byte, 32); //RX_32Byte is a global variable } else if (type == W) { //FET_Control, REG12_Control TX_Reg[2] = data & 0xff; I2C_WriteReg(0x3E,TX_Reg,3); delayUS(1000); TX_Buffer[0] = Checksum(TX_Reg, 3); TX_Buffer[1] = 0x05; //combined length of registers address and data I2C_WriteReg(0x60, TX_Buffer, 2); delayUS(1000); } else if (type == W2){ //write data with 2 bytes //CB_Active_Cells, CB_SET_LVL TX_Reg[2] = data & 0xff; TX_Reg[3] = (data >> 8) & 0xff; I2C_WriteReg(0x3E,TX_Reg,4); delayUS(1000); TX_Buffer[0] = Checksum(TX_Reg, 4); TX_Buffer[1] = 0x06; //combined length of registers address and data I2C_WriteReg(0x60, TX_Buffer, 2); delayUS(1000); } } void DirectCommands(uint8_t command, uint16_t data, uint8_t type) // See the TRM or the BQ76952 header file for a full list of Direct Commands { //type: R = read, W = write uint8_t TX_data[2] = {0x00, 0x00}; //little endian format TX_data[0] = data & 0xff; TX_data[1] = (data >> 8) & 0xff; if (type == R) {//Read I2C_ReadReg(command, RX_data, 2); //RX_data is a global variable delayUS(2000); } if (type == W) {//write //Control_status, alarm_status, alarm_enable all 2 bytes long I2C_WriteReg(command,TX_data,2); delayUS(2000); } } void BQ769x2_Init() { // Configures all parameters in device RAM // Enter CONFIGUPDATE mode (Subcommand 0x0090) - It is required to be in CONFIG_UPDATE mode to program the device RAM settings // See TRM for full description of CONFIG_UPDATE mode CommandSubcommands(SET_CFGUPDATE); // After entering CONFIG_UPDATE mode, RAM registers can be programmed. When programming RAM, checksum and length must also be // programmed for the change to take effect. All of the RAM registers are described in detail in the BQ769x2 TRM. // An easier way to find the descriptions is in the BQStudio Data Memory screen. When you move the mouse over the register name, // a full description of the register and the bits will pop up on the screen. // 'Power Config' - 0x9234 = 0x2D80 // Setting the DSLP_LDO bit allows the LDOs to remain active when the device goes into Deep Sleep mode // Set wake speed bits to 00 for best performance BQ769x2_SetRegister(PowerConfig, 0x2D80, 2); // 'REG0 Config' - set REG0_EN bit to enable pre-regulator BQ769x2_SetRegister(REG0Config, 0x01, 1); // 'REG12 Config' - Enable REG1 with 3.3V output (0x0D for 3.3V, 0x0F for 5V) BQ769x2_SetRegister(REG12Config, 0x0D, 1); // Set DFETOFF pin to control BOTH CHG and DSG FET - 0x92FB = 0x42 (set to 0x00 to disable) BQ769x2_SetRegister(DFETOFFPinConfig, 0x42, 1); // Set up ALERT Pin - 0x92FC = 0x2A // This configures the ALERT pin to drive high (REG1 voltage) when enabled. // The ALERT pin can be used as an interrupt to the MCU when a protection has triggered or new measurements are available BQ769x2_SetRegister(ALERTPinConfig, 0x2A, 1); // Set TS1 to measure Cell Temperature - 0x92FD = 0x07 BQ769x2_SetRegister(TS1Config, 0x07, 1); // Set TS3 to measure FET Temperature - 0x92FF = 0x0F BQ769x2_SetRegister(TS3Config, 0x0F, 1); // Set HDQ to measure Cell Temperature - 0x9300 = 0x07 BQ769x2_SetRegister(HDQPinConfig, 0x00, 1); // No thermistor installed on EVM HDQ pin, so set to 0x00 // 'VCell Mode' - Enable 16 cells - 0x9304 = 0x0000; Writing 0x0000 sets the default of 16 cells BQ769x2_SetRegister(VCellMode, 0x0000, 2); // Enable protections in 'Enabled Protections A' 0x9261 = 0xBC // Enables SCD (short-circuit), OCD1 (over-current in discharge), OCC (over-current in charge), // COV (over-voltage), CUV (under-voltage) BQ769x2_SetRegister(EnabledProtectionsA, 0xBC, 1); // Enable all protections in 'Enabled Protections B' 0x9262 = 0xF7 // Enables OTF (over-temperature FET), OTINT (internal over-temperature), OTD (over-temperature in discharge), // OTC (over-temperature in charge), UTINT (internal under-temperature), UTD (under-temperature in discharge), UTC (under-temperature in charge) BQ769x2_SetRegister(EnabledProtectionsB, 0xF7, 1); // 'Default Alarm Mask' - 0x..82 Enables the FullScan and ADScan bits, default value = 0xF800 BQ769x2_SetRegister(DefaultAlarmMask, 0xF882, 2); // Set up Cell Balancing Configuration - 0x9335 = 0x03 - Automated balancing while in Relax or Charge modes // Also see "Cell Balancing with BQ769x2 Battery Monitors" document on ti.com BQ769x2_SetRegister(BalancingConfiguration, 0x03, 1); // Set up CUV (under-voltage) Threshold - 0x9275 = 0x31 (2479 mV) // CUV Threshold is this value multiplied by 50.6mV BQ769x2_SetRegister(CUVThreshold, 0x31, 1); // Set up COV (over-voltage) Threshold - 0x9278 = 0x55 (4301 mV) // COV Threshold is this value multiplied by 50.6mV BQ769x2_SetRegister(COVThreshold, 0x55, 1); // Set up OCC (over-current in charge) Threshold - 0x9280 = 0x05 (10 mV = 10A across 1mOhm sense resistor) Units in 2mV BQ769x2_SetRegister(OCCThreshold, 0x05, 1); // Set up OCD1 Threshold - 0x9282 = 0x0A (20 mV = 20A across 1mOhm sense resistor) units of 2mV BQ769x2_SetRegister(OCD1Threshold, 0x0A, 1); // Set up SCD Threshold - 0x9286 = 0x05 (100 mV = 100A across 1mOhm sense resistor) 0x05=100mV BQ769x2_SetRegister(SCDThreshold, 0x05, 1); // Set up SCD Delay - 0x9287 = 0x03 (30 us) Enabled with a delay of (value - 1) * 15 s; min value of 1 BQ769x2_SetRegister(SCDDelay, 0x03, 1); // Set up SCDL Latch Limit to 1 to set SCD recovery only with load removal 0x9295 = 0x01 // If this is not set, then SCD will recover based on time (SCD Recovery Time parameter). BQ769x2_SetRegister(SCDLLatchLimit, 0x01, 1); // Exit CONFIGUPDATE mode - Subcommand 0x0092 CommandSubcommands(EXIT_CFGUPDATE); } // ********************************* FET Control Commands *************************************** void BQ769x2_BOTHOFF () { // Disables all FETs using the DFETOFF (BOTHOFF) pin // The DFETOFF pin on the BQ76952EVM should be connected to the MCU board to use this function P4OUT |= BIT2; // DFETOFF pin (BOTHOFF) set high } void BQ769x2_RESET_BOTHOFF () { // Resets DFETOFF (BOTHOFF) pin // The DFETOFF pin on the BQ76952EVM should be connected to the MCU board to use this function P4OUT &= ~BIT2; // DFETOFF pin (BOTHOFF) set low } void BQ769x2_ReadFETStatus() { // Read FET Status to see which FETs are enabled DirectCommands(FETStatus, 0x00, R); FET_Status = (RX_data[1]*256 + RX_data[0]); DSG = ((0x4 & RX_data[0])>>2);// discharge FET state CHG = (0x1 & RX_data[0]);// charge FET state PCHG = ((0x2 & RX_data[0])>>1);// pre-charge FET state PDSG = ((0x8 & RX_data[0])>>3);// pre-discharge FET state } // ********************************* End of FET Control Commands ********************************* // ********************************* BQ769x2 Power Commands ***************************************** void BQ769x2_ShutdownPin() { // Puts the device into SHUTDOWN mode using the RST_SHUT pin // The RST_SHUT pin on the BQ76952EVM should be connected to the MCU board to use this function P2OUT |= BIT3; // Set RST_SHUT pin } void BQ769x2_ReleaseShutdownPin() { // Releases the RST_SHUT pin // The RST_SHUT pin on the BQ76952EVM should be connected to the MCU board to use this function P2OUT &= ~BIT3; // Reset RST_SHUT pin } // ********************************* End of BQ769x2 Power Commands ***************************************** // ********************************* BQ769x2 Status and Fault Commands ***************************************** uint16_t BQ769x2_ReadAlarmStatus() { // Read this register to find out why the ALERT pin was asserted DirectCommands(AlarmStatus, 0x00, R); return (RX_data[1]*256 + RX_data[0]); } void BQ769x2_ReadSafetyStatus() { //good example functions // Read Safety Status A/B/C and find which bits are set // This shows which primary protections have been triggered DirectCommands(SafetyStatusA, 0x00, R); value_SafetyStatusA = (RX_data[1]*256 + RX_data[0]); //Example Fault Flags UV_Fault = ((0x4 & RX_data[0])>>2); OV_Fault = ((0x8 & RX_data[0])>>3); SCD_Fault = ((0x8 & RX_data[1])>>3); OCD_Fault = ((0x2 & RX_data[1])>>1); DirectCommands(SafetyStatusB, 0x00, R); value_SafetyStatusB = (RX_data[1]*256 + RX_data[0]); DirectCommands(SafetyStatusC, 0x00, R); value_SafetyStatusC = (RX_data[1]*256 + RX_data[0]); if ((value_SafetyStatusA + value_SafetyStatusB + value_SafetyStatusC) > 1) { ProtectionsTriggered = 1; } else { ProtectionsTriggered = 0; } } void BQ769x2_ReadPFStatus() { // Read Permanent Fail Status A/B/C and find which bits are set // This shows which permanent failures have been triggered DirectCommands(PFStatusA, 0x00, R); value_PFStatusA = (RX_data[1]*256 + RX_data[0]); DirectCommands(PFStatusB, 0x00, R); value_PFStatusB = (RX_data[1]*256 + RX_data[0]); DirectCommands(PFStatusC, 0x00, R); value_PFStatusC = (RX_data[1]*256 + RX_data[0]); } // ********************************* End of BQ769x2 Status and Fault Commands ***************************************** // ********************************* BQ769x2 Measurement Commands ***************************************** uint16_t BQ769x2_ReadVoltage(uint8_t command) // This function can be used to read a specific cell voltage or stack / pack / LD voltage { //RX_data is global var DirectCommands(command, 0x00, R); if(command >= Cell1Voltage && command <= Cell16Voltage) {//Cells 1 through 16 (0x14 to 0x32) return (RX_data[1]*256 + RX_data[0]); //voltage is reported in mV } else {//stack, Pack, LD return 10 * (RX_data[1]*256 + RX_data[0]); //voltage is reported in 0.01V units } } void BQ769x2_ReadAllVoltages() // Reads all cell voltages, Stack voltage, PACK pin voltage, and LD pin voltage { unsigned char x; int cellvoltageholder = Cell1Voltage; //Cell1Voltage is 0x14 for (x = 0; x < 16; x++){//Reads all cell voltages CellVoltage[x] = BQ769x2_ReadVoltage(cellvoltageholder); cellvoltageholder = cellvoltageholder + 2; } Stack_Voltage = BQ769x2_ReadVoltage(StackVoltage); Pack_Voltage = BQ769x2_ReadVoltage(PACKPinVoltage); LD_Voltage = BQ769x2_ReadVoltage(LDPinVoltage); } uint16_t BQ769x2_ReadCurrent() // Reads PACK current { DirectCommands(CC2Current, 0x00, R); return (RX_data[1]*256 + RX_data[0]); // current is reported in mA } float BQ769x2_ReadTemperature(uint8_t command) { DirectCommands(command, 0x00, R); //RX_data is a global var return (0.1 * (float)(RX_data[1]*256 + RX_data[0])) - 273.15; // converts from 0.1K to Celcius } void BQ769x2_ReadPassQ(){ // Read Accumulated Charge and Time from DASTATUS6 Subcommands(DASTATUS6, 0x00, R); AccumulatedCharge_Int = ((RX_32Byte[3]<<24) + (RX_32Byte[2]<<16) + (RX_32Byte[1]<<8) + RX_32Byte[0]); //Bytes 0-3 AccumulatedCharge_Frac = ((RX_32Byte[7]<<24) + (RX_32Byte[6]<<16) + (RX_32Byte[5]<<8) + RX_32Byte[4]); //Bytes 4-7 AccumulatedCharge_Time = ((RX_32Byte[11]<<24) + (RX_32Byte[10]<<16) + (RX_32Byte[9]<<8) + RX_32Byte[8]); //Bytes 8-11 } //****************************************************************************** // main ************************************************************************ //****************************************************************************** int main(void) { // Stop watchdog timer WDTCTL = WDTPW | WDTHOLD; // Initialize GPIOs, clocks and peripherals GPIO_initPins(); UCS_initModule(); __no_operation(); I2C_initModule(); CommandSubcommands(BQ769x2_RESET); // Resets the BQ769x2 registers delayUS(60000); BQ769x2_Init(); // Configure all of the BQ769x2 register settings delayUS(10000); CommandSubcommands(FET_ENABLE); // Enable the CHG and DSG FETs delayUS(10000); CommandSubcommands(SLEEP_DISABLE); // Sleep mode is enabled by default. For this example, Sleep is disabled to // demonstrate full-speed measurements in Normal mode. delayUS(60000); delayUS(60000); delayUS(60000); delayUS(60000); //wait to start measurements after FETs close /* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { /* USER CODE END WHILE */ /* USER CODE BEGIN 3 */ //Reads Cell, Stack, Pack, LD Voltages, Pack Current and TS1/TS3 Temperatures in a loop //This basic example polls the Alarm Status register to see if protections have triggered or new measurements are ready //The ALERT pin can also be used as an interrupt to the microcontroller for fastest response time instead of polling //In this example the LED on the microcontroller board will be turned on to indicate a protection has triggered and will //be turned off if the protection condition has cleared. AlarmBits = BQ769x2_ReadAlarmStatus(); if (AlarmBits & 0x80) { // Check if FULLSCAN is complete. If set, new measurements are available BQ769x2_ReadAllVoltages(); Pack_Current = BQ769x2_ReadCurrent(); Temperature[0] = BQ769x2_ReadTemperature(TS1Temperature); Temperature[1] = BQ769x2_ReadTemperature(TS3Temperature); DirectCommands(AlarmStatus, 0x0080, W); // Clear the FULLSCAN bit } if (AlarmBits & 0xC000) { // If Safety Status bits are showing in AlarmStatus register BQ769x2_ReadSafetyStatus(); // Read the Safety Status registers to find which protections have triggered if (ProtectionsTriggered & 1) { P1OUT |= BIT0; } // Turn on the LED to indicate Protection has triggered DirectCommands(AlarmStatus, 0xF800, W); // Clear the Safety Status Alarm bits. } else { if (ProtectionsTriggered & 1) { BQ769x2_ReadSafetyStatus(); if (!(ProtectionsTriggered & 1)) { P1OUT &= ~BIT0; } } // Turn off the LED if Safety Status has cleared which means the protection condition is no longer present } delayUS(20000); // repeat loop every 20 ms } } void GPIO_initPins() { // Initialize all pins to output low, except P4.5 P1OUT = 0x00; P2OUT = 0x00; P3OUT = 0x00; P4OUT = 0x00; P5OUT = 0x00; P6OUT = 0x00; P1DIR = 0xFF; P2DIR = 0xFF; P3DIR = 0xFF; P4DIR = 0xFF; P5DIR = 0xFF; P6DIR = 0xFF; // Configure GPIOs GPIO_configPins(); // Disable the GPIO power-on default high-impedance mode to activate // previously configured port settings PM5CTL0 &= ~LOCKLPM5; } void GPIO_configPins() { /* Inputs */ // Button S1 P4DIR &= ~BIT1; // Set P4.1 as input P4REN |= BIT1; // Enable internal resistor P4OUT |= BIT1; // Set pull-up on this pin // Button S2 P2DIR &= ~BIT3; // Set P2.3 as input P2REN |= BIT3; // Enable internal resistor P2OUT |= BIT3; // Set pull-up on this pin /* Outputs */ // P1.0 (LED1) P1OUT &= ~BIT0; // Set P1.0 to low P1DIR |= BIT0; // Set P1.0 to output direction // P6.6 (LED2) P6OUT &= ~BIT6; // Set P6.6 to low P6DIR |= BIT6; // Set P6.6 to output direction } void UCS_initModule() { #ifdef __ENABLE_XT1__ // Configure XT1 pins P2SEL0 |= BIT6 | BIT7; do { CSCTL7 &= ~(XT1OFFG | DCOFFG); // Clear XT1 and DCO fault flags SFRIFG1 &= ~OFIFG; }while (SFRIFG1 & OFIFG); // Test oscillator fault flag #endif // Configure one FRAM waitstate as required by the device datasheet for MCLK // operation beyond 8MHz _before_ configuring the clock system. FRCTL0 = FRCTLPW | NWAITS_1; // Clock System Setup __bis_SR_register(SCG0); // Disable FLL #ifdef __ENABLE_XT1__ CSCTL3 |= SELREF__XT1CLK; // Set XT1 as FLL reference source #else CSCTL3 |= SELREF__REFOCLK; // Set REFO as FLL reference source #endif CSCTL0 = 0; // clear DCO and MOD registers CSCTL1 &= ~(DCORSEL_7); // Clear DCO frequency select bits first CSCTL1 |= DCORSEL_5; // Set DCO = 16MHz CSCTL2 = FLLD_0 + 487; // DCOCLKDIV = 16MHz __delay_cycles(3); __bic_SR_register(SCG0); // Enable FLL Software_Trim(); // Software Trim to get the best DCOFTRIM value #ifdef __ENABLE_XT1__ CSCTL4 = SELMS__DCOCLKDIV | SELA__XT1CLK; // MCLK = SMCLK = DCO; ACLK = XT1 (external) #else CSCTL4 = SELMS__DCOCLKDIV | SELA__REFOCLK; // MCLK = SMCLK = DCO; ACLK = REFO (internal) #endif } void I2C_initModule() { // Configure I2C pins __no_operation(); P1SEL0 |= BIT2 | BIT3; P1SEL1 &= ~(BIT2 | BIT3); // Configure I2C peripheral UCB0CTLW0 = UCSWRST; // Enable SW reset UCB0CTLW0 |= UCMODE_3 | UCMST | UCSSEL__SMCLK | UCSYNC; // I2C host mode, SMCLK UCB0BRW = 40; // fSCL = SMCLK/40 = ~400kHz UCB0I2CSA = DEV_ADDR; // Device Address UCB0CTLW0 &= ~UCSWRST; // Clear SW reset, resume operation UCB0IE |= UCNACKIE; } void UART_initPins() { // Configure UART pins, module is configured in HAL_GUIComm_UART_FR235x.c P4SEL0 |= BIT2 | BIT3; P4SEL1 &= ~(BIT2 | BIT3); } void Software_Trim() { unsigned int oldDcoTap = 0xffff; unsigned int newDcoTap = 0xffff; unsigned int newDcoDelta = 0xffff; unsigned int bestDcoDelta = 0xffff; unsigned int csCtl0Copy = 0; unsigned int csCtl1Copy = 0; unsigned int csCtl0Read = 0; unsigned int csCtl1Read = 0; unsigned int dcoFreqTrim = 3; unsigned char endLoop = 0; do { CSCTL0 = 0x100; // DCO Tap = 256 do { CSCTL7 &= ~DCOFFG; // Clear DCO fault flag }while (CSCTL7 & DCOFFG); // Test DCO fault flag __delay_cycles((unsigned int)3000 * CPU_FREQ_MHZ); // Wait FLL lock status (FLLUNLOCK) to be stable // Suggest to wait 24 cycles of divided FLL reference clock while((CSCTL7 & (FLLUNLOCK0 | FLLUNLOCK1)) && ((CSCTL7 & DCOFFG) == 0)); csCtl0Read = CSCTL0; // Read CSCTL0 csCtl1Read = CSCTL1; // Read CSCTL1 oldDcoTap = newDcoTap; // Record DCOTAP value of last time newDcoTap = csCtl0Read & 0x01ff; // Get DCOTAP value of this time dcoFreqTrim = (csCtl1Read & 0x0070)>>4;// Get DCOFTRIM value if(newDcoTap < 256) // DCOTAP < 256 { newDcoDelta = 256 - newDcoTap; // Delta value between DCPTAP and 256 if((oldDcoTap != 0xffff) && (oldDcoTap >= 256)) // DCOTAP cross 256 endLoop = 1; // Stop while loop else { dcoFreqTrim--; CSCTL1 = (csCtl1Read & (~DCOFTRIM)) | (dcoFreqTrim<<4); } } else // DCOTAP >= 256 { newDcoDelta = newDcoTap - 256; // Delta value between DCPTAP and 256 if(oldDcoTap < 256) // DCOTAP cross 256 endLoop = 1; // Stop while loop else { dcoFreqTrim++; CSCTL1 = (csCtl1Read & (~DCOFTRIM)) | (dcoFreqTrim<<4); } } if(newDcoDelta < bestDcoDelta) // Record DCOTAP closest to 256 { csCtl0Copy = csCtl0Read; csCtl1Copy = csCtl1Read; bestDcoDelta = newDcoDelta; } }while(endLoop == 0); // Poll until endLoop == 1 CSCTL0 = csCtl0Copy; // Reload locked DCOTAP CSCTL1 = csCtl1Copy; // Reload locked DCOFTRIM while(CSCTL7 & (FLLUNLOCK0 | FLLUNLOCK1)); // Poll until FLL is locked } //****************************************************************************** // I2C Interrupt *************************************************************** //****************************************************************************** #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__) #pragma vector = USCI_B0_VECTOR __interrupt void USCI_B1_ISR(void) #elif defined(__GNUC__) void __attribute__ ((interrupt(USCI_B0_VECTOR))) USCI_0_ISR (void) #else #error Compiler not supported! #endif { // Must read from UCB0RXBUF uint8_t rx_val = 0; switch(__even_in_range(UCB0IV, USCI_I2C_UCBIT9IFG)) { case USCI_NONE: break; // Vector 0: No interrupts case USCI_I2C_UCALIFG: break; // Vector 2: ALIFG case USCI_I2C_UCNACKIFG: // Vector 4: NACKIFG break; case USCI_I2C_UCSTTIFG: break; // Vector 6: STTIFG case USCI_I2C_UCSTPIFG: break; // Vector 8: STPIFG case USCI_I2C_UCRXIFG3: break; // Vector 10: RXIFG3 case USCI_I2C_UCTXIFG3: break; // Vector 12: TXIFG3 case USCI_I2C_UCRXIFG2: break; // Vector 14: RXIFG2 case USCI_I2C_UCTXIFG2: break; // Vector 16: TXIFG2 case USCI_I2C_UCRXIFG1: break; // Vector 18: RXIFG1 case USCI_I2C_UCTXIFG1: break; // Vector 20: TXIFG1 case USCI_I2C_UCRXIFG0: // Vector 22: RXIFG0 rx_val = UCB0RXBUF; if (RXByteCtr) { ReceiveBuffer[ReceiveIndex++] = rx_val; RXByteCtr--; } if (RXByteCtr == 1) { UCB0CTLW0 |= UCTXSTP; } else if (RXByteCtr == 0) { UCB0IE &= ~UCRXIE; MasterMode = IDLE_MODE; __bic_SR_register_on_exit(CPUOFF); // Exit LPM0 } break; case USCI_I2C_UCTXIFG0: // Vector 24: TXIFG0 switch (MasterMode) { case TX_REG_ADDRESS_MODE: UCB0TXBUF = TransmitRegAddr; if (RXByteCtr) MasterMode = SWITCH_TO_RX_MODE; // Need to start receiving now else MasterMode = TX_DATA_MODE; // Continue to transmission with the data in Transmit Buffer break; case SWITCH_TO_RX_MODE: UCB0IE |= UCRXIE; // Enable RX interrupt UCB0IE &= ~UCTXIE; // Disable TX interrupt UCB0CTLW0 &= ~UCTR; // Switch to receiver MasterMode = RX_DATA_MODE; // State state is to receive data UCB0CTLW0 |= UCTXSTT; // Send repeated start if (RXByteCtr == 1) { // Must send stop since this is the N-1 byte while((UCB0CTLW0 & UCTXSTT)); UCB0CTLW0 |= UCTXSTP; // Send stop condition } break; case TX_DATA_MODE: if (TXByteCtr) { UCB0TXBUF = TransmitBuffer[TransmitIndex++]; TXByteCtr--; } else { // Done with transmission UCB0CTLW0 |= UCTXSTP; // Send stop condition MasterMode = IDLE_MODE; UCB0IE &= ~UCTXIE; // Disable TX interrupt __bic_SR_register_on_exit(CPUOFF); // Exit LPM0 } break; default: __no_operation(); break; } break; default: break; } }