This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: How can automative balancing can run if two AFE in series

Part Number: BQ76952


Tool/software:

Dear All,

I am using two AFEs in series to make it 32S, but if each IC knows only its own max and min cell voltage, is there any way to run automatic cell balancing in both AFE with respect to one minimum cell voltage?

  • Hello Raja,

    As the IC only knows its own max and min cell voltage, it should not be able to automatically cell balance for both AFEs with respect to one minimum cell voltage. With host controlled cell balancing, this is more possible.

    Best Regards,
    Alexis