Part Number: BQ35100
Tool/software:
Hi team,
Please tell me some of them.
Q. In EOS mode, the sequence of sending GAUGE_START() 1 second before high load pulse, sending GAUGE_STOP() immediately after pulse stop, and waiting for G_DONE is shown.
but does this need to be done every time to get the current EOS value?
Q. Regarding the high load pulse mentioned above, it is stated that a voltage drop of 100mV or more is required under load compared to no load. Is there any limitation on the pulse length?
Q. TRM 5.3.1 states that NEW_BATTERY() must be executed when changing batteries. What happens if it is not executed?
Q. Other than setting CHEM_ID, what should be set for the BQ35100 IC on each board?
Best Regards,
Ryu.