This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65219-Q1: Review of PMIC_LPM_EN0 Connection

Part Number: TPS65219-Q1

Tool/software:

Hello TI Experts,

Our OTP for the PMIC is 20W. Due to some of the features requested by customers, the EN/PB/SENSE of the PMIC to AM62x SOC was connected in a way that it resembled 2 wired-OR, along with PMIC_LPM_EN0 signal from the SOC, as shown in the picture. The two wired-ORs were connected to external wake up factor respectively.

My question is that: if both the SOC and the 2 wake up factors try to enable the PMIC at the same time (all signal HIGH), would there be any concern/effect to this?