Tool/software:
My Schematic shown as below.

I would like to ask about the datasheet 7.4.7 Standalone Versus Host Interface(pg 29). From this section, I know that this chip which able to use standalone mode. I am using standalone mode to activate the chip, but I have facing some issue. In 7.8.1 Overview of Operational Modes, there are 4 modes. Based on this section, I obtain deep sleep mode results as REGOUT LDO is 3.3V;CHG is 0.5V and DSG is 0V through multimeter.
1. May I know what is the actual initial state of this IC as I cant found or miss out in the datasheet?
2. Is it necessary to include the circuit shown as below to let deep sleep mode become normal mode if using standalone mode to activate it as I did not include this part in my circuit which shown in the pg 43 datasheet.

3. If no included the circuit that shown in question 2, so need to have at least TS pin or VC0 connect to MCU digital pin for wake up(for shutdown mode)?
Thanks in advance.