This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSF12C1: TPSF12C1

Part Number: TPSF12C1

Tool/software:

Hello

I have to develop a Switch mode power supply, with multiple outputs. Each output needs its own reference therefore I was thinking of a flyback topology.

The output requirements are 24vdc 10A: 36 Vdc 0.5A: 5Vdc 2A and another 24Vdc 2.5A. Do you have any buck converter chips which already have some of these requirements, so I do not have to develop the converter with micro processor etc?

Or do you have any experience to pick the right coil to handle all these outputs? should i pick one with many possbilities or multiply coils?

Best Regards Lasse