Tool/software:
Hello,
We'd like to increase the sense resistor on the BQ25731 to 20mohm.
Is this possible?
Or will RSNS_RAC and RSNS_RSR cause a problem?
Thank you, Keith
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello,
We'd like to increase the sense resistor on the BQ25731 to 20mohm.
Is this possible?
Or will RSNS_RAC and RSNS_RSR cause a problem?
Thank you, Keith
Hi, Keith,
Yes, the customer can use 20mohm. The charger does not use the absolute value of RSNS_RAC/RSNS_RSR for IBAT/ISYS/IBUS/PSYS calculation.
It leaves for the customer to interpret the readback value, sometime, we need to scale-up or scale-down regarding the current setting or current feedback.
However, please keep the RAC/RSR ratio as 1:1, 1:2 or 2:1. This ratio will affect the PSYS calculation.
For example, if both RAC=RSR=20mohm, leave RSNS_RAC=RSNS_RSR=10mohm.
1A charge current setting (0x0200) *10mohm =0.5A *20mohm.
Programm charge current register 0x0200, now set the charge current to 0.5A.
Regards,
Tiger