Other Parts Discussed in Thread: GPCRB
Tool/software:
Hi ti team
7870.Gauge settings_Panasonic_NCR2170M_ID7473_KAYO_20250106.gg.csvI have a product using the BQ27Z746. It is in a 1S2P configuration with a voltage of 4.2V and a capacity of 9100mAh at room temperature. However, when I charge the battery to 4.2V in a low-temperature environment of 0°C, due to the low temperature, the capacity of the battery when charged to 4.2V at 100% SOC is only about 7500mAh. When I restore the temperature to 25°C and start discharging, the BQ27Z746 will mistakenly think that the full charge capacity (FCC) is 9100mAh. But in fact, at this time, only about 7500mAh of capacity can be discharged. This will cause the state of charge (SOC) to jump. I would like to ask if there is any way to solve this scenario where charging is done at 0°C in a low-temperature environment and discharging is carried out at 25°C in a high-temperature environment.
Thanks