Other Parts Discussed in Thread: UCC27710
Tool/software:
Hi sir,
What's TI P2P solution with FAN7387MX
Thanks a lot!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey Sean,
Thank you for reaching out to TI with your questions regarding a P2P solution.
It appears that the FAN7387MX has been discontinued.
It is a half-bridge gate driver with a self oscillating operation that is rated for 625V with 0.35A / 0.65A of drive current.
The closest option that we have is the UCC27710 which is a 620V driver with 0.5A / 1.0A of drive current but it does not have the self oscillator. It features independent inputs for the high-side and low-side.
Let me know if there are further questions.
Thank you,
William Moore