Tool/software:
Hello,
I would like to realize a modulable constant current source. The current control was previously done with a linear regulator. This is to be changed in order to reduce waste heat. The operating voltage would be 3-12V, the current should be externally adjustable via a 0..10V source and the secondary should be 0/5mA to 3A.
My approach would be a switching regulator as a current source, a shunt in front of the consumer with a differential amplifier and thus an influence on the feedback from the switching regulator. The load would be one or more LEDs in series. The Modulation Speed via 0..10V should be as fast as possible.
Thanks for every Tip or Idea.
Greetings
calibra