Tool/software:
Hello team,
I need to know maximum inrush current capability of TPS1HB35-Q1 if it need to handle a capacitive load in the range of 1128uF to 5280 uF.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello team,
I need to know maximum inrush current capability of TPS1HB35-Q1 if it need to handle a capacitive load in the range of 1128uF to 5280 uF.
Hello,
The TPS1HB35 is not recommended for capacitive load charging. When the device hits current limit it will disable the switch immediately.

Devices for capacitive charging applications it is recommended to use the TPS1HA08 or the TPS1HC08 as they clamp the current when limiting happens rather than immediately shutting off the switch.
For the capacitance listed the inrush will be really high.
BR,
Alan
Hello , Thanks for the information . I have a query whether TPS1HB08 Can also be used instead of TPS1HA08 for the above capacitive loading applications?
Hey,
The HB device family has the same functionality. When it hits current limit it will shut off the TPS1HB08 will not have the same capacitive load charging as TPS1HA08.
BR,
Alan