This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM51770: How to use with FETs that has integrated gate drivers?

Part Number: LM51770
Other Parts Discussed in Thread: LMG3100R017

Tool/software:

Hello, I'm trying to design a buck-boost converter with the LMG3100R017, a GaN FET with built in gate drivers. But the LM51770 also has built in gate drivers, which causes a conflict. What is the correct way to make them work together? Maybe there's some way to bypass the gate driver that I couldn't find? Use an LDO? Using a microcontroller feels wrong since then I'd have to do all the control in code. Or are there control chips without integrated gate drivers? I don't seem to able to filter by that. I see there are HO1_LL and HO2_LL but I'm not sure that's how they're supposed to be used, as well as having no counterparts for the low side. Please advise, thanks a lot.