This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM61460-Q1: POWER_EN is connected to 24V through a 10K resistor. An output of 8V appears instantly upon power-up, and then the chip burns out immediately. The VIN of the chip is burned out. Is there a problem with the schematic diagram?

Part Number: LM61460-Q1


Tool/software:

 POWER_EN is connected to 24V through a 10K resistor. An output of 8V appears instantly upon power-up, and then the chip burns out immediately. The VIN of the chip is burned out. Is there a problem with the schematic diagram?