This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2623: LM2623AMM/NOPB Vin 4.5V to 9V

Part Number: LM2623
Other Parts Discussed in Thread: TLV61047

Tool/software:

Hi TI,

sorry to bother you, it seems I cannot use your device properly.

I would like to obtain a 9V from a Vin that has a min of 4.1V and a max of 4.9V (as output of BQ24079QWRGTTQ1).
The components are the same one of the datasheet, aside from the resistors Rf1 and Rf2 that are respectively 316KOhm and 50KOhm.

I see an output of 7.8V (very stable) and the FB pin drop to a 1V voltage.
I tried changing the capacitor on the frequency pin and to change resistors but the output stay at 7.8V.

I noticed that I reach a 1.23V voltage on the FB pin only if I turn up the Vin to 7V (sometimes even to 8, depending on the resistors ratio).

Any idea on what's happening? Have I reached a current cap?

Thank you for your advices!

Chiara

  • Hello Chiara,

    Please try doubling C24. It is possible that you trip the duty cycle or inductor current limit with this low value. See this part of the datasheet: www.ti.com/.../datasheet

    Best regards,
    Brigitte

  • Hello!

    Thank you for your reply.

    Unluckly, I tried using 10pF, a 47pF a 100pF and then a 220pF as C24 capacitor (as TI talked about the difficulty in choosing the right mesure) but the results are always the same.

    I saw a little improvement by removing C8, something I found odd.

    To be more accurate, I leave here some results, if they have any meaning for you:

    • With C8 as written, C24 70pF, V pin FB = 0.940V and Vout=7.77V
    • Without C8, C24 70pF, V pin FB =0.984V and Vout=7.9V
    • With C8 as written, C24 220pF, V pin FB =0.9V and Vout=7.76V

    Thank you for your help

    Chiara

  • Hi Chiara,

    Is there a load at output when you test? If the load is heavy, the Vout cannot reach the target.

  • Hi!

    No, I have no load attached.

    I tried simulating a load with a resistor to see if something changed... But nothing happened.
    I'll try to test it today, on an old buy where it worked before. Right now I can only think of a problem with the pcb itself.
    I'll let you know if I see some results but I'll take any advice you have.

  • Hi Chiara,

    Do you try C24 as 4.7pF or 3.3pF? And you can try R16+R31+R35 larger to get lower frequency.

    Besides, I recommend our new product TLV61047, which is easy to use.