This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54160A: Leaving EN pin floating when TPS54160A used as an inverting pwr supply

Part Number: TPS54160A
Other Parts Discussed in Thread: TPS54160,

Tool/software:

Hi,
I'm using the TPS54160ADRCR as an inverting pwr supply, from +24V to -6V following the SWIFTINV-CALC-REVE.xls excel sheet and the SLVA317B document instructions. The TPS54160 datasheet says that the EN pin has an internal pull-up current source and if left floating it enables the IC, is it ok to leave EN floating when using the TPS54160A as an inverting pwr supply?