This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62901-Q1: EN input level compatibility

Part Number: TPS62901-Q1


Tool/software:

Section 7.5 in the datasheet show the EN pin has 0.97 < VIH < 1.03V. I'm using a number of this dc/dc converter to generate 5v and 1v supplies. If the PGOOD is pulled-up to 5v and drives the EN pin of the 1V dc/dc, will this exceed the EN limit of the 1v dc/dc? Does VIN of the 1v dc/dc affect the EN input max voltage?