Other Parts Discussed in Thread: GPCCHEM
Tool/software:
Hello,
I've used the GPCCHEM tool to generate valid chemistries for our system. I'm a little confused on the results that we got. The cells we are using in our 16S1P pack are 5.04Ah cells with a maximum voltage of 4.2V for each, but the report from the chemistry tool is suggesting that the best match is an ID for a 3216mAh cell and in the description it has 4.3V listed. Does this sounds correct? Should I look for a different chemistry in the list that is closer to the 5040mAh, 4.2V cell we are actually using?
Also, I ran 2 different chemID cycles, one using a single cell and another using a whole pack. Each report generated a different chemistry list. Which report should I reference when choosing a chemistry to program?
Thanks,
Jordan