This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP2992: PCN Legacy Chip and the New Chip

Part Number: LP2992

Tool/software:

Hi All,


I have a question about LP2992.
The PCN has added information about the Legacy Chip and the New Chip.
Will I need to change the design if I change from the Legacy Chip to the New Chip?

The capacitor information for the Legacy Chip says to use a capacitor with a low ESR (5mΩ),
but the New Chip allows up to 1Ω, so I don't think I will need to change the design if I change from the Legacy Chip to the New Chip.
Am I understanding this correctly?


Best Regards,
Ishiwata