This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS16630-32EVM: UL rating for TPS16630 : 4.5-V to 60-V, 31mΩ, 0.6-6A eFuse

Part Number: TPS16630-32EVM
Other Parts Discussed in Thread: TPS1663

Tool/software:

Hello Expert ,

We are using TPS16630 in our design and front end protection for 48V , 6A input line.

This product has to qualify for UL rating for 48V operation.

Can you please confirm whether TPS16630RGET is UL certified for 48V operation ?

Its operating voltage is 4.5V to 60 V and datasheet mentions about UL certified .

Thanks

Regards

Vasu