This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25756: Voltage rating of MOSFETs

Part Number: BQ25756

Tool/software:

I've got a design in progress using the BQ25856. To date, I was expecting 12-24V on the input side and 15-18V on the output side. In this particular case, the supply will only be used in forward mode, never in reverse to get power back from the output side. All my FET's are 40V FETs. Now I've been asked to support 48V input, but still have the 15-18V output. I found the 80V version of my FETs. My first thought is that I only need to change out the input side FET's for the higher voltage. Because this is a last minute change, I'd like a bit of confirmation so I don't mess it up. It seems so obvious that I have to ask.