dear Sir...
we had question to TPS65251's operation condition.
if we did disconnect the 1 Vin line,
it can good operation about remain 2 output...
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
dear Sir...
we had question to TPS65251's operation condition.
if we did disconnect the 1 Vin line,
it can good operation about remain 2 output...
Lee,
The VIN pin is the input supply and it provides the power to operate the IC. There must be power provided to this pin (4.5V-18V).
Converters 1, 2, 3 are individually powered through VIN1, VIN2, and VIN3.
If there is no power being provided to VIN1, and there is power being provided to VIN2 and VIN3, the output voltage from converter 2 and converter 3 should be operating correctly based on your external component design.