Other Parts Discussed in Thread: TPS22953
Tool/software:
Hello TI Experts,
Section 10.1.3 of the TPS22965 datasheet indicates that a Cin greater than CL is highly recommended due to the current flow through the body diode from Vout to Vin. In my design, the CL is 330 uF, Cin is 1 uF also CT is 1 nF. The Input is 5V, and the maximum current is 3A. How much reverse current can TPS22965 handle? Will damage occur to the chip due to reverse current ?
ZHIYAR TAHIR