Other Parts Discussed in Thread: PMP10344, UCC256302
Tool/software:
Hi ,
We are looking for the AC to DC rectifier design for the below specification for our new product development,
Input voltage: 3phase voltage 110/220/230/240/380/400/415/460/ 480VAC. (Or) Single Phase voltage 110, 220, 230 & 240 VAC
& Input voltage: 24VDC ( if possible on the same single board design)
Output voltage : 24VDC @ 6A (Output1) & 12VDC @ 2A (optional)
I can see couple of example reference design like PMP10344 support such a design specification. Please guide me the proper flyback switching ICs from where to start for the above request.
Regards,
Ravi