Tool/software:
Hi,
in our application we are using lithium thionyl chloride 38Ah. (two cells in parallel). my questions are
1) during the normal operation/measurement, what happens if VREGIN, goes to zero, does the chip lose all battery measured data, calibration etc?
2)
![]()

i see that the maximum voltage difference between SRP and SRN should be 125mV, does it related to load pulse voltage drop ?
in our application pulse load voltage drop could be 500mV (e.g 3.5V to 3.0) for 200ms, so in this case we will exceed the limit of 125mV between SRP and SRN ?
3) does BQ35100 is valid for the application where the voltage drop is variable (100mV to 500mV) everytime during the day ?
Thanks.
Afzal