Tool/software:
I want to use the TPS7A89 such that Vin = 5.6V and Vout=5V, for each of its two outputs (on at the same time).
I want to keep the junction temp of the whole part below 100C. when I calculate the Trise, should I use the total current (sum of the current from each of its outputs) or should I be doing that calculation with only the max current from each LDO output?
So, for example, if Rja = 33 dec/W, and I am supplying 1A from each output of this part, is the Trise = (0.6) X (1A) x 33 = 19.8 deg C ?