Other Parts Discussed in Thread: TPS92515, LM3406
Tool/software:
First time working with the TPS92515(HV) and I'm just working out that the delivered current is dependent on the inductor ripple current, which is then dependant on the inductance which is most cases is tolerance to +/-20%.
If I'm designing around an 82uH inductor with a tolerance of 20% then values of between 66uH to 98uH should be expected.
In my 48V -> 17V, 217KHz, 1A design I can expect the following inductor ripple., 98uH = 49%, 66uH = 73%.
When I target 82uH = 1.0A, then at 98uH I get 1.05A, and at 66uH I get 0.93A
Any tricks I'm missing to get a more tightly controlled drive current? I suppose running the converter faster with a smaller inductor would help, but I'm trying to eek out efficiency in my design.