Tool/software:
Hello!
I think there is an issue with this circuit or behaviour of the eFuse. When I connect a 24V in through the main switch, there is the same voltage between the eFuse EN/UVLO and GND terminals. However, the output seems to be pulled LOW.

The values I have selected for the resistors and capacitors are:
| Rvl1 | 1 MOhm |
| Rvl2 | 9.091 kOhm |
| Cin | 0.1 uF |
| CNRetry | 2.2 nF |
| CRetry_delay | 2.2 nF |
| RI_lim | 115 Ohm |
| CiTimer | NC |
| CdVdt | 3.9 nF |
| Rimon | 1050 Ohm |
| Rpg | 10 kOhm |
| COUT | 100 uF |
I selected these to have a current limit of 13A. When I tested this, I only had a minor load across the OUT, for a DCDC powering a small <1A component. The test results were:
Vin = 25V
Vout = LOW.
Please let me know if I have made a mistake or if you need any more information to help me fix this issue. Thank you!