Other Parts Discussed in Thread: TL431
Tool/software:
Hello,
I'm using UCC25600 for LLC converter with the following specifications:-
Input Voltage :- 665Vdc
Switching Frequency :- 100kHz
Output Voltage :- 55V
Output Power :- 150W
I'm using Tina model of this to simulate it but the output voltage doesn't reach 55V as per requirements.
1) I've set the Tank values as per calculations giving in SLUP263 document.
Considering Q=0.56, Lm/Lr=5, Dead time :- 500nsec
2) I've set the feedback resistors such that at 55V output, I get 2.5V reference at TL431.
3) Can you also help me out with the component values for Over Current protection.
I've attached the Tina simulation file as well FYR.
Thanking you in advance,
Regards,
Dilip R