Tool/software:
Hi there, i have a set of ten prototypes with the LMR54406 mounted.
It is used to generate a 5V from 24V.
Problem is: three of the ten prototypes are not working correctly. There is no voltage regulation and input equals output, so instead of 5V i have 24V at the output.
Is there anything i can do ? I already changed one of the LMRs with a newer one, but same problem.
Best wishes
Martin