This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS629203: question about TPS629203

Part Number: TPS629203

Tool/software:

Hello:

As discussed earlier, TI has recommended TPS629203,as follows:

(+) TPS62120: Question about TPS62120 - Power management forum - Power management - TI E2E support forums

now The current customer engineer's test results for TPS629203 are as follows:
Input 7.201V current 0.5429228mA, output 3.3V, current 1mA, efficiency=83.80%
However, when the input is 7.201V, the output is 2V, and 1mA, it reaches around 79%
The customer's application scenario is 2V. Please help analyze the reasons or recommend more suitable materials. Thank you!

Please refer to the thread above for specific requirements