This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC33420: Isolated Power Supply Recomendation for 24 to 96V Battery System

Part Number: UCC33420
Other Parts Discussed in Thread: UCC14241-Q1

Tool/software:

Hello,

I entered a random product code just to get a product recommendation.

We are looking for an isolated supply for a 3-phase motor driver system that steps down from a vehicle battery voltage range of 24V to 96V to 12V output, providing 4A source and 8A sink gate driver per phase, and using 8 FETs in parallel per phase.

Can you recommend a suitable isolated DC-DC converter for this system?

Best regards,

Egemen