Other Parts Discussed in Thread: REF50, REF50E
Tool/software:
What happens to the output of the REF02 if a higher current is sunk into the output pin?
As an example, if a 10k resistor is connected between the output pin and a 30V source. This would presumably require the REF02 to sink 2.5mA, but the datasheet says a typical sinking load current is 0.5mA - but this is not listed as an "absolute maximum". What does the output do in this situation?