Tool/software:
Hi,
We would appreciate your confirmation on the following three points regarding the BQ25172 device behavior:
-
The datasheet defines both rising and falling thresholds for VOUT_OVP, suggesting a hysteresis mechanism.
Could you confirm whether the device terminates charging when the output voltage exceeds the rising threshold (e.g., 1.70 V/cell), and resumes charging when the voltage drops below the falling threshold (e.g., 1.45 V/cell)? -
Our understanding is that VRECHG serves as the voltage threshold to initiate recharge when intermittent charging is enabled. Is this correct?
-
When intermittent charging is disabled, it appears that the device still resumes charging once the battery voltage drops below VRECHG.
Is it correct to say that VRECHG is used internally as the recharge trigger even in non-intermittent mode?
Also, are there any other voltage thresholds that can trigger a recharge cycle?
Thanks,
Conor