This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM74700-Q1: IC for Power ORing

Part Number: LM74700-Q1
Other Parts Discussed in Thread: LM74500-Q1,

Tool/software:

I am referring to two IC's --LM74500-Q1 and LM74700-Q1. 

In the LM74700-Q1 datasheet it's application has Power ORing. 

Which feature makes LM74700-Q1 to be used for power ORing?.

Can we use LM74500-Q1 for power ORing?.

What is the difference between those two devices?

In addition to that, Is it okay if enable(20V) comes before the input at ANODE?[Is it Failsafe?]