Tool/software:
Hi support team,
Currently being evaluated with TPS63901EVM.
I checked the operation during soft-start and found something that concerned me.
TPS63901_Soft-Start_250509.xlsx
It is set to increase from 1.8V to the set value (3.9V in this case) in 100mV steps, but I found that the input current increases and the input voltage drops with each step.
I have a few questions about this operation.
[Question]
1. Please let me know what causes the input current to increase. I would like to understand what is happening inside the TPS63901.
2. Please let me know how to reduce the input voltage drop.
3. I have confirmed that setting the Input Current Limit reduces the input voltage drop, but is this the correct way to do it?
4. Is it possible to change the Input Current Limit after the output voltage has been set?
For example, I could prepare two resistors for the Input Current Limit setting and switch between them.
Regards,
Dice-K