This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7H1121-SP: Footprint of TPS7H1121MPWPTSEP TSSOP 24 Pin Package and Thermal Pad Issue

Part Number: TPS7H1121-SP


Tool/software:

Does the TPS7H1121MPWPTSEP package contains E-Pad(Thermal Pad) under the package?

If so I could not find footprint in the datasheet, Could you provide me a footprint drawing of TPS7H1121MPWPTSEP (TSSOP 24Pin) device?

  • Hello,

    Yes, the package for that part will have a thermal pad. For now since the part is only in preview, you can find the footprint drawing at the end of the datasheet of any other TI part that uses the same package. Here is a link to package lookup tool which displays other parts with the 24-pin PWP package.

    Thanks,

    Sarah