Part Number: UCC21710-Q1
Tool/software:
Hi everyone,
The reason why I'm asking is because the datasheet is a bit vague on that aspect. In table 5.9 the test conditions for the input high and input low voltages are VCC = 3.3V for the logic inputs.
However at the top of that page it states that the table is applicable for both 5V and 3.3V applications. So I just want to make sure, can the UCC21710QDWRQ1 be powered on VCC with 5V, whilst having 3.3V PWM, RDY, FLT and RST#EN signals. Thanks!