Other Parts Discussed in Thread: BQ79600-Q1
Tool/software:
Dear Team
1. What happens if we update the cell balancing timers before expiration and send the Go Command?
2. Suppose I write three cells' cell balancing timers with a non-zero value, but one of the three cells reaches the VCB_Done_Threshold value, will the rest of the two cells balance, or will it raise a cell balancing fault
3. Is there any other 16-bit or 2 8-bit register to control 16 Cell Balancing FETS of the device?
4. Say if I want to turn on CB_FET1 and turn off all other Channels, I have to set a non-zero value for CB_FET1 and all other zero, later if I want to turn off CB_FET1 and turn on CBFET2 I have to set a non-zero value to CBFET2 and all other zero, and GO Command. Am I right?
5. I am able to read all registers except BAL_STAT ( I can read cell voltages, temperatures ). Command sent to read Balancing Status:A0 05 2B 00 2C D5 . Please check
Thanks& Regards
Mounish