Other Parts Discussed in Thread: LMV431, TLV803E, TLV431, TLVH431, TL431, LM25037, TL331B
Tool/software:
Hi!
I would like to use an LMV431 as a comparator. My question is: When REF < 1.24V (i.e., when the output is at a high logic level), how much current flows through the cathode?
I have created a quick example circuit to illustrate my question. 
If no current flows through the cathode, then half of the supply voltage can be measured across R4.
However, some current does flow through the cathode, which changes the voltage drop across R4.
If I understand the datasheet correctly, this might be the "Minimum cathode current for regulation," which is typically 55 µA.
Please help me clarify this question.