Other Parts Discussed in Thread: BQSTUDIO
Tool/software:
I am using the BQ34Z100-G1. And the battery is also working well.
However, I have been operating it for over two month, but the cycle count has not changed.
I would like to ask when the cycle count changes. I thought that the cycle count would increase when the current flowing through the battery accumulates and exceeds the CC threshold.
I will explain the operation after the installation of the product.
The battery's status was initially over 40%. Then it gradually charged with the solar panels and reached about 90%.
Since then, it has been changing between 60% and 90% for over a month. However, the cycle count is still 0.
When will the cycle count increase?
I will add my data memory file (*.gg) .
thank you.