Tool/software:
Hi team,
Is it possible to limit the inrush current to below 500mA with this device?
The USB Power-Distribution Requirements in section 10.2.3.1.1 state "Limit inrush current (<44 Ω and 10 µF)." Does this mean that if Rilim is less than 44Ω, it can handle the inrush current?
Additionally, are there similar devices with better (newer) supply availability? Regarding the TPS25221, is it a product that can be used long-term without any supply issues?
Best regards,
Kyohei