Tool/software:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi Tanaka-san,
The device shouldn't require a specific startup sequence. Could you check if ASC_EN_PRI, ASC_EN_SEC, or any of the GDx pins are being driven high?
Regards,
Max Verboncoeur
Hello Maxwell,
Thank you for explaining the startup sequence. I understand that there is no specific startup sequence, which leads me to believe that the issue lies with the IC terminal inputs.
Current Status: We are verifying the initial operation of the gate driver IC with the minimal configuration (testing without SPI communication).
Therefore, we are testing whether the PWM signal can be output using only GDx and INP & INN.
Additional Questions: The port settings of the IC currently being tested are as follows. If there are any mistakes in the settings, please advise.
GDx Terminals:
ASC Terminals:
Reference: Other Terminal Settings
OUTH1, OUTH2, OUTL1, OUTL2: Connected to 0.02uF assuming MOSFET gate capacitance.
Hi Tanaka-san,
Could you check the status of the nFLTx pins? If there is no fault, then they should be high.
Also, VCP should normally be above VCC2. What is the value of the decoupling cap between VCP and VCC2?
Regards,
Max Verboncoeur
Hello Maxwell!
The nFLT is 3.5V for both nFLT1 and nFLT2.
*Both pins are measured at the voltage after passing through the RC filter (100Ω) with the pins unconnected.
The pull-up resistor inside the IC and the voltage divider of 100Ω are measured, can they be considered Hi state? (VCC1=5V)
VCP and VCC2 are connected with only 0.1μF decoupling capacitor.
*Datasheet P98 recommends a decoupling capacitor of 0.01uF to 0.1uF (0603 size, etc.).
The capacitor used is CGA4J2X8R1H104K125AE, which has a capacitance of 0.1µF but a size of 2012
Both VCC2 and VCP are +18.0V, and there is almost no potential difference between VCP and VCC2.
I believe that the GDIC terminal input outputs are fine except for the OUTH output, but am I missing something?
Hi Tanaka-san,
Would you be able to share a waveform of your PWM, the GDx pins, and the OUTx signal?
Regards,
Max Verboncoeur
Hi Maxwell-san,
sorry for the delay in getting back to you.
I found the cause of the problem with the gate driver IC that I was discussing with you.
The cause was found to be the pattern in which the gate driver IC is mounted.
After correcting the pattern, the IC is working fine as shown in the attached figure.
Red: PWM input (function generator output)
Light blue: Gate driver IC output
Now that we know that there is no problem with the gate driver IC and that it operates normally, please let me complete this question.